STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Motor Control Issue with MCSDK 6.4.0

Hello,I am working with the STM32F303E-EVAL control board and the STEVAL-IPMNM2S power board, using IAR Embedded Workbench 9.40.I have struggled to get the motor running. I initially tried both MCSDK versions 9.3.2 and 9.4.0 separately, but in most c...

Resolved! Motor pilot firmware for EVLSERVO1 board

Hello,I had the motor profiling experience to get motor mechanical and electrical parameters using EVSPIN32G4 boardsas following:Now I'm trying to start the project for controlling a new high power motor with EVLSERVO1 board. But, I couldn't find the...

rokkie68_1-1757497951533.png rokkie68_0-1757497369140.png
rokkie68 by Associate
  • 986 Views
  • 1 replies
  • 0 kudos

Resolved! Motor forward/reverse transition issue in ST Motor Pilot

Hi all,I’m currently using the EVSPIN32G4 development board for a drone project. I’m controlling motor forward and reverse using ST Motor Pilot.I’ve noticed that when switching from forward to reverse, there’s a short pause before the motor starts sp...

1123 by Associate II
  • 981 Views
  • 1 replies
  • 0 kudos

Resolved! STSPIN32G4 integrate buck convertor

Hello, I am developing a custom board with the STSPIN32G4 microcontroller.I would like to have more information about the integrated buck converter, as the documentation lacks details.What is the maximum allowed peak current? Output curent 12V :  Bes...

Cedd_0-1757320554088.png
Cedd by Associate II
  • 892 Views
  • 1 replies
  • 1 kudos

Driver protection for custom inverter board

Hi Team,I'm working on design the custom inverter board for 3 Phase BLDC Motor for rail door application.Motor driver these feature needed for project In motor Driver protection this one im using  In Phase voltage generation TIM8 using and the motor ...

VINODC_0-1757074655240.png VINODC_1-1757074709660.png VINODC_2-1757074732425.png
VINODC by Associate II
  • 740 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.