2025-09-11 10:02 PM
Hello,
How do I determine the power rating for Vcc input to STIB1560DM2T-LZ.
Regards,
PiPPiP
2025-09-12 2:52 AM
Hello @PiPPiP,
You can refer to the STEVAL-IPMM15B board, which is based on the STIB1560DM2T-L SLLIMM™ product.
2025-09-12 3:57 AM
Yep, have looked at that at length - is there an easy answer? 1A perhaps?
2025-09-14 4:51 PM
Or failing an easy answer, can you help me work out what the rating should be from the figures in the quoted dev board (I spent the weekend looking and could not work it out).
Thanks
PiPPiP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.