2022-04-20 11:48 PM
Are there any plans to make a Linux version of the Motor Control Workbench.
2022-04-25 2:02 AM
Hello @Sune Jensen,
Yes, the technology used in MCSDK6.0.0 is now cross-platform and Linux versions are in the pipe.
Regards
Cedric
2022-04-27 4:54 PM
How about a Mac version? Same story?
Mike
2023-12-13 2:25 AM
Seeing that all released versions of MCSDK6 still only supports windows, do you have any new information about the timeline for Linux support?
2024-08-20 1:08 AM - edited 2024-08-20 1:08 AM
Any updates on this? We are still only able to download the Windows-version.
2025-09-04 8:37 AM
Hi @cedric H
Its been a while since you said the Linux version is in the pipe. Is there any progress? Seems it must be quite a long pipe.. Realistically is this ever going to happen? It is very inconvenient having to support a seperate machine just to support the motor workbench, it really would be very helpful to be able to manage the whole project on Linux instead of only half.
Thanks.
Clive
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.