STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Motor suddenly turns in the wrong direction

 [PN]: Customer Board (Very similiar IHM08M1 and STM32G431RB)[VERSION]: 6.3.1[TOOL]: Motor Pilot[DETAILS]: at heavy load step the motor turns suddenly in wrong direction with full speed (see plot below)[EXPECTED BEHAVIOR]: stable speed or motor stops...

RReic2_0-1755679708505.png RReic2_1-1755679993144.png
RReic.2 by Associate II
  • 1667 Views
  • 10 replies
  • 0 kudos

spin3204 hall sensor speed feedback issue

Hello,I’m testing a motor with integrated Hall sensors for which I don’t have the datasheet and that I can’t disassemble. From the tests I’ve done, it appears to be a 4-pole motor with Hall sensors spaced 120 mechanical degrees apart.I first tested t...

Screenshot 2025-08-22 092847.png Screenshot 2025-08-22 091809.png Screenshot 2025-08-22 090214.png Screenshot 2025-08-22 090206.png
VILLO by Associate II
  • 608 Views
  • 1 replies
  • 0 kudos

EVSPIN32G4-DUAL board takes very large current

[PN]: EVSPIN32G4-DUAL, STSPIN32G4, STDRIVE101[VERSION]: 6.4.0[TOOL]: Motor Control Workbench[DETAILS]:When I start the motor from motor pilot, even though I have set low peak currents (0.2A) in the project, on startup more than 1.8A is taken from the...

GSB by Associate II
  • 1028 Views
  • 8 replies
  • 0 kudos

Motor controller not connecting

Hey STM community,I have a G431RB & IHM16M1 however whenever i try to run the motor pilot, i cant seem to connect to the board. I  have made sure all the necessary link drivers are installed, i have made the baudrate  115200, 8bit all to match up wit...

Screenshot 2025-08-31 213103.png
Gath0004 by Associate
  • 443 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.