2025-09-04 7:01 AM
Hi Team,
I have design for the custom inverter for the STM32G4A1VET6 controller and motor driver is Infineon.
custom board is designed and the while generating the code getting error as "1.4.0psdc: PSDC Version is not supported"
while I tried to download this package manually couldn't download showing error "FP-SNS-STBOX1" support package.
2025-09-04 7:22 AM
According to me if the project .c files are generated successfully then you can neglect the warnings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.