STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

MCSDK & Motor Profiler with low RPM BLDC motor

Posted on May 01, 2018 at 22:23Hello,I am trying to use the MCSDK to control a 250W BLDC motor. Here the the specification.Electrical 36V nom, 7 amps max, 10 pole pairs.Mechanical ~ 8 N.m, and no more than 300 RPM.I am using the F302R8 and IHM08M1 i...

0690X0000060ArYQAU.png

Any example on how to use MCSDK 5.0?

Posted on May 15, 2018 at 03:11The 5.0 version use commands like 'bool MC_StartMotor1(void);' instead of the old 4.3 'bool MCI_StartMotor(CMCI this);' This api change is documented in AN5143 rev 2.A google search on MC_StartMotor1 gives one hit - in...

Motor Profiler fails

Posted on May 21, 2018 at 16:58My end aim is to use #Motor #profiler to workout my motor parameters. I have #nucleo-F302R8 and #X-nucleo-IHM08M1 boards.I selected these two in Profiler, Connected My motor and Hall devices, Entered 4 Pole pairs and m...

dsystem by Associate II
  • 955 Views
  • 1 replies
  • 0 kudos

How to use Motor Profiler with STEVAL-ESC001V1

Posted on June 03, 2018 at 09:43I am trying to use the STEVAL-ESC001V1 with the motor profiling tool but I can't get the motor profiler to connect to the controller. I am using a ST-LINK/V2 with the STSW-LINK009 driver on Win7. I am able to connect ...

Comms failure on MCWB

I have a STEVAL-SPIN3202 programmed and configured for FOC, and a small motor which has been profiled by the profiler and an ESC001V1. Code is auto generated by MCWB and compiled using Eclipse (I have to change the min_stack_size to 0x300 because MCW...

STEVAL-ESC001v1 - Motor profiler - profiling failed

Hello,I have tried to use Motor Profiler with ESC001v1 and drone rc outrunner motor: 14n12p (7 pole pairs), 6s, 600kvConnection via St-link and Uart was succesfull, firmware uploaded to the board ESC001v1, but motor profiling failed.Where could be a...

Kamil1 by Associate III
  • 2121 Views
  • 3 replies
  • 1 kudos

MotorProfiler with different board set

Hello, I would like to know if there's a way to use the motor profiler with a different set of board then the predefine one. I already have the NUCLEO-F302R8 and now i want to use it with a STEVAL-IPM07F. The MotorWorkbench tools allows me to use bot...

PFeit by Associate
  • 1030 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.