STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Motor profiler and delta connected windings

In all fan motors that we like to profile the three windings are delta connected.The motor profiler runs but states at the end that the resistances and inductivities are out of the range of supported values. Is there a possibility to switch the behav...

HLewo by Associate
  • 890 Views
  • 1 replies
  • 0 kudos

Motor charakterisation using NucleoF302R8 and IHM07/08

Dear Ladies and Gentleman, as a research project to find a smart and easy way to characterize different brush-less DC-motors, we are working with your NucleoF302R8 and IHM07/08 circuits.To begin with, we started using the "ST Motor Profiler" to profi...

leo.r by Associate II
  • 2966 Views
  • 6 replies
  • 0 kudos

Motor Profiler Connection error

Hi,I have a stm32f769i-eval board and steval028v2. I look the UM2035 and did some modification on stm32f769i. After than i connected the boards each other and pc.I start the motor profiler but didnt work. I get a error. I connect on STlink port to pc...

0690X00000AQxkPQAT.png 0690X00000AQxkKQAT.png
trgyada by Associate II
  • 1225 Views
  • 1 replies
  • 0 kudos

X-NUCLEO IHM07M1 - Motor Profiler Problem

I bought a F401RE and an IHM07M1 to work on the subject BLDC a couple of weeks ago but, I could not profile the motor. My motor is T-Motor U8 170kw. It has 36 coils and 42 poles. I connected my boards successfully but, when I clicked "Start Profile" ...

0690X00000AqOy9QAF.jpg

Resolved! STM32G431CB Source code ?

Hy there,I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. af...

N_1 by Associate II
  • 4878 Views
  • 14 replies
  • 0 kudos

Unable to run high rpm bldc motor using Motor profiler

I have a Nucleo - F302R8 board with X-Nucleo - IHM07M1 BLDC motor driver. I'm trying to drive my bldc motor which is Emax rs 1106 - 6000kv using motor profiler software.Using the motor profiler software with suitable settings (pole pair = 6 , Max Spe...

HMoos by Associate
  • 1633 Views
  • 4 replies
  • 1 kudos

Motor Profiler doesn't work for Emax motors

Dear ST team,I have a Nucleo - F302R8 board with X-Nucleo - IHM07M1 BLDC motor driver. I'm trying to drive my bldc motor which is Emax rs 1106 - 6000kv using motor profiler software.Using the motor profiler software with suitable settings (pole pair ...

0690X000008ACYeQAO.png 0690X000008ACYZQA4.png
HMoos by Associate
  • 867 Views
  • 1 replies
  • 0 kudos

Delay when changing motor rotation?

Hy there,I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. af...

N_1 by Associate II
  • 1020 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.