2018-12-03 12:26 AM
Hello,
I have tried to use Motor Profiler with ESC001v1 and drone rc outrunner motor: 14n12p (7 pole pairs), 6s, 600kv
Connection via St-link and Uart was succesfull, firmware uploaded to the board ESC001v1, but motor profiling failed.
Where could be a problem? How can get more information than only "profile failed" ?
Thank you
Kamil
2020-02-19 2:44 AM
Getting same error with
STEVAL-IPM15B + NUCLEO-F303RE + X-NUCLEO-IHM09M1
Have you found any solution?
2020-05-14 10:01 AM
unfortunatelly I haven't found any solution, absolutely no answer or help from ST...
2021-06-27 9:55 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.