2018-06-03 12:43 AM
I am trying to use the STEVAL-ESC001V1 with the motor profiling tool but I can't get the motor profiler to connect to the controller. I am using a ST-LINK/V2 with the STSW-LINK009 driver on Win7. I am able to connect to the controller using the STM32 ST-LINK Utility so I think the wiring is correct and I am missing something on the motor profiler side of things. Any ideas on what the issue might be? I am getting 'Connection Error! Please, check the connection between the board and PC.'
2018-07-03 8:52 AM
Correct. You also need a USB->serial adapter connected to the UART pins. They are unfortunately 1.27mm pitch so it's a bit fiddly.
2021-06-27 9:57 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.