2018-12-05 2:25 PM
Hello,
I would like to know if there's a way to use the motor profiler with a different set of board then the predefine one.
I already have the NUCLEO-F302R8 and now i want to use it with a STEVAL-IPM07F. The MotorWorkbench tools allows me to use both board but not the motorprofiler.
Is there a way to tweak the motorprofiler to support other boards set?
Thanks,
Pascal
2018-12-30 12:53 PM
Hello,
The only boards supported by the profiler are the ones they allow you to choose from the program (this was emphasized in a class for the MC workbench). We have used one of the stock board combinations listed to profile a motor however. When you save that motor profile, it is accessible by the motor workbench. So you can still use that profile, it is just generated by their boards.
Mr Yan
2021-06-27 9:54 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.