STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Voltage unit clarification

Dear MCSDK team,Could you clarify SDK conversion from Volts to s16v.In UM2392 document it says that 1s16v = VMAX / 32768 -> s16v = V * 32768 / VMAXIn MC Parameters Calculations document / Current Controllers slide, it says that Gains in V / A are con...

ANICO.1 by Associate III
  • 1745 Views
  • 2 replies
  • 0 kudos

Hi, I'm using STM32G431KBT6 board. I couldn't get PWM complementary output to drive stepper motor (28byj-48 5VDC). How can I do that ?

I'm using TIM1 pwm generation ch1 ch1n & ch2 ch2n. My deadtime is set to 200. It's running at 100Hz and %50 duty cycle. I set the parameters as it should but nothing is working. My channel 1 & channel 2 settings are the same. Can someone help me to d...

0693W00000HohgwQAB.jpg 0693W00000HohghQAB.jpg
SÖzde.1 by Associate
  • 1044 Views
  • 1 replies
  • 0 kudos

Overload Derating

I want to know the overload based derating, there will be continuous current and the peak current. If the current exceeds continuous current for a certain duration i consider overload. What to be done i do not know. Does ST has any application notes?

JDesi.1 by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

STEVAL IHM034V2 evaluation board, three phase induction motor is not running, PWN and IPM module is not working

Hi,i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).i am using three phase induction motorwell I am using the Motor Control Workbench 5.4.7, for generating code , Keil uVision5 for burring the code in Controller ,  the code is bu...

MAhme.5 by Associate
  • 2375 Views
  • 1 replies
  • 0 kudos
GSeme.1 by Associate II
  • 2163 Views
  • 2 replies
  • 0 kudos

How I connect to Steval-IPM15B ?

I have Nucleo-F302R8T6 and STEVAL-IPM15B. But I don't know how to connect the pins. I tried to connect it by looking at the pins from the Motor control workbench program, but some pins were exposed, RX, TX pins were exposed. Can you help me how to c...

Eakso.1 by Associate II
  • 2053 Views
  • 2 replies
  • 0 kudos

Weired output then OC, and controller damaged

Hi all,​I am using f303rb with ihm08-1sh to control a motor, motor control is MCSDK 5.3.2Using HSI which has 64MHz clock speed.I set the PWM frequency to 15K, and FOC execution rate = 2.In most time, it works okay.In a very low probability, it will O...

0693W00000HpcxzQAB.bmp
JHSU.16 by Associate
  • 1688 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.