2021-12-26 1:57 AM
I want to know the overload based derating, there will be continuous current and the peak current. If the current exceeds continuous current for a certain duration i consider overload. What to be done i do not know. Does ST has any application notes?
2021-12-31 7:11 AM
Dear @JDesi.1
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
And eventually more details about your application...
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.