STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Error

  i installed x-cube sdk  then  i wanted to make project for an example but even tough i installed last version of cube mx program but i am taked that things all the time thanks for your help.

erenyurdagul_0-1763999039863.png

Resolved! Program not running after power cycle

[VERSION]: MCWB v6.3.2[TOOL]: STM32CubeMX v6.13.0, STM32CubeIDE v1.11.5[BOARD]: STEVAL-PTOOL1V1[PROJECT]: STEVAL-PTOOL1V1_6S_SL and STEVAL-PTOOL1V1_6S_HLWhen I run the STEVAL-PTOOL1V1_6S_SL project generated by STM32CubeMX, the program loads and runs...

STM32CubMX not found in MC Workbench 6.3.2

Hello,I saw that some people had a similar problem to mine. When generating the project on MC Workbench I have the following error: STM32CubeMX not found - ver. "6.0.0" or higher is requiredBut I have STM32CubeMX installed with version 6.14.0I tried ...

Xavier75_0-1741023700517.png Xavier75_1-1741023826780.png Xavier75_2-1741023948130.png
Xavier75 by Associate II
  • 2434 Views
  • 7 replies
  • 0 kudos

Inerzia and fiction brushless motor

Hi, I wanted to ask a question about brushless and MCSDK motors. When buying a motor, inertia is often listed, but friction isn't. Can I calculate friction using inertia, or is friction a parameter that can be omitted?

SDall by Associate II
  • 602 Views
  • 3 replies
  • 0 kudos

Closed loop ihmi08

Hi, I'm using the boatd ihmi08. I would like to control the motor in closed loop as a target rotor angle. Is it possible in 6 steps or is the focus much better?

SDall by Associate II
  • 542 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.