STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

The project does not build in "CubeIDE".

Development environmentMotor control workbench Version: 6.4.0STM32CubeMX Version: 6.16.0STM32CubeIDE Version: 2.00.0Controler/Driver: B-G431B-ESC1 kitI want to drive a 30W BLDC motor using the B-G431B-ESC1 kit.I'm currently following the instructions...

realcrew by Associate II
  • 691 Views
  • 3 replies
  • 0 kudos

Resolved! MCSDK STSPIN32g4 disable via Vcc

Hello,I'm working with a custom board that uses an external 12V supply for the VCC pin (gate driver supply) of STSPIN32g4. The VCC supply is interrupted by external circuitry whenever a fault is detected.The problem I'm encoutering is that when the 1...

Favand by Associate II
  • 764 Views
  • 4 replies
  • 1 kudos

Current Sensing

Current Sensing的这两个参数应该怎么填,该如何计算得到,或者有官方文档介绍吗?How should these two parameters for Current Sensing be filled in? How should they be calculated? Or is there any official documentation available?

Ethan_hu_0-1764573490318.png
Ethan_hu by Associate
  • 352 Views
  • 1 replies
  • 0 kudos

Why the motor start with MC_OVER_CURR error?

Hi there,I have a DIY board similar to EVSPIN32G4. Below is the three-shunt sensing circuit(In internal OpAmps, differential, external gain mode)Because the STSPING4 doesn't support internal OpAmps, differential, external gain mode, I just use the be...

Junde_0-1764138125903.png Junde_1-1764138515887.png Junde_2-1764138530032.png
Junde by Senior III
  • 824 Views
  • 2 replies
  • 0 kudos

HSO Overmodulation

Hello! I saw in the release notes for MCSDK 6.4.0 that there is an "Added new Maximum Modulation Index (MMI) computation compatible for all sensor-less or sensor algorithms." How should I use overmodulation on the HSO?

WJHuang by Associate
  • 532 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.