cancel
Showing results for 
Search instead for 
Did you mean: 

Inerzia and fiction brushless motor

SDall
Associate II

Hi, I wanted to ask a question about brushless and MCSDK motors. When buying a motor, inertia is often listed, but friction isn't. Can I calculate friction using inertia, or is friction a parameter that can be omitted?

3 REPLIES 3
Gael A
ST Employee

Hello SDall,

Friction and inertia are mechanical characteristics of the motor that are used for PID Speed Gains determination. We provide a piece of software called the MotorProfiler to estimate those two values and compute the Speed PID gains. You can find more information on our wiki : https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:STM32_MC_Motor_Profiler_-_Start-up_guide

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

So is it important for the Hall sensors to be connected to the motor profile process? I tried without, but the configuration got stuck halfway and wouldn't continue.

Gael A
ST Employee

Hello SDall,

Hall sensor connection is not mandatory for profiling your motor. If the profiling takes too much time or gets stuck, don't hesitate to tinker with the speed and current values to see if the behaviour improves.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.