2025-10-16 6:15 AM
Since Updating to new Version is always a lot of manual work i would kindly ask for a Change Log compared to the Major Version 6.4.0.
The new Features / Improvements may justify/not justify the move from 6.4.0 -> 6.4.1.
Solved! Go to Solution.
2025-10-21 6:16 AM
Hello @StefanH1,
A post is available on the homepage of the ST Motor control forum (as for MCSDK6.4.0) for main changes description.
This post is not available for the MCSDK6.4.1 version. Once downloaded, refer to the V6.4.1 main changes chapter in the Release Notes documentation available through Workbench tool > About > Documentations.
2025-10-21 6:16 AM
Hello @StefanH1,
A post is available on the homepage of the ST Motor control forum (as for MCSDK6.4.0) for main changes description.
This post is not available for the MCSDK6.4.1 version. Once downloaded, refer to the V6.4.1 main changes chapter in the Release Notes documentation available through Workbench tool > About > Documentations.
2025-10-24 4:55 AM - edited 2025-10-24 4:57 AM
Thanks for your answer. I hoped for a easier solution than downloading and installing the latest version to get that Information.
2025-11-24 12:52 PM
i extracted release notes and posting here:
This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) is a bug fix release of the version 6.4.0.
Please note that the MCSDK executable is provided as a ST digitally signed executable.
Taking the opportunity of this new release, several topics reported through ST Community have been fixed :
Description ST Community links
| TIM8 configuration does not work with 6step project | MCSDK6.3.2 GenerateCode Error about TIM8 |
| BEMF ADC sampling time not taken from MCWB | Why are 3 ADC pins configured in 6-step BLDC SDK, but only Channel 13 is used in injected mode? |
| Hall sensor not working on 6.4 | Hall sensor not working on 6.4 |
| Speed Loop PID Tuning in ESC001V1 | Speed Loop PID Tuning in ESC001V1 |
In addition to the fixes mentioned above, this delivery brings the following improvements :
6Step algorithm:
FOC algorithm:
Fixed issue on ADC polarization affecting 1shunt topology for cortex M0/M0+ series (STM32C0, STM32G0, STM32F0)
Added ability to use Encoder and Hall sensors at the same time (main and auxiliary) (functionality available on specific B-G473E-ZEST1S board)
Hall sensors are not locked anymore in "Not Reliable" state if they are back on track. It allows a smooth STO-PLL -> Hall sensors dynamic transition.
Specific changes introduced in the ST Motor Control Workbench
Specific changes introduced in the ST Motor Control Board Manager
Specific changes introduced in the ST Motor Control Board Designer
Specific changes introduced in the ST Motor Pilot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.