STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! STM32 Motor Control SDK -V6.41

Hai All,  New to the workbench software.  Able to set the required parameters - STM32F446RE & IHM08M1.  Getting stuck in the final path - CubeMx & IDE.   But I am having the latest updated one.   Kindly help me where I am missing.Jayaraj.A

Recommended Voltage Margin für STSPIN32G0

Hello ST communityWhat voltage margin would you suggest if using the motor STSPIN32G0A2 controller IC ? The supply voltage of the IC is rated from 15-45V. Is it safe to supply it with 36V and connect a BLDC motor to it? I am scared that the IC may be...

Review of Custom STSPIN32G4 Schematic

Hi everyone,I’m new to STM32 and working on a custom board using the STSPIN32G4 to drive a 3-phase BLDC motor (max 1000 W). The board will be powered by a 7-cell Li-ion pack (max 29.4 V, up to 30 A). I would appreciate a general schematic review.Coul...

ElGuerrero91_0-1765139629378.png Screenshot 2025-12-07 194032.png

Operating the STEVAL-ESC002V1 with 8S battery?

I am curious what dictates the operating conditions of the STEVAL-ESC002V1 to a 2-6S battery and 20A current capability? I would like to use this chipset and operate from an 8S battery. The specs state that the MCU is capable of operating up to 45V a...

hoser by Associate
  • 430 Views
  • 1 replies
  • 0 kudos

How can I configure the board under senseless mode?

Hello Everybody,Here are the software and boards in this case:1. MC workbench 6.3.22. STEVAL-IHM039V1/STEVAL-CTM009V1I have an I-PMSM motor, and I use the board (STEVAL-IHM039V1/STEVAL-CTM009V1) to run the ST Motor Pilot for spinning the motor. Howev...

039V1_senseless_startupFault.jpg
DF_MC by Associate III
  • 672 Views
  • 2 replies
  • 0 kudos

What is the most likely cause of the motor noise?

Hello Everybody,Here are the software and boards in this case:1. MC workbench 6.3.22.STEVAL-IHM039V1/STEVAL-CTM009V1I am using an I-PMSM motor with the ST development boards (STEVAL-IHM039V1 / STEVAL-CTM009V1). In open-loop mode, the motor spins smoo...

039V1_009V1_hall.jpg
DF_MC by Associate III
  • 741 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.