2014-08-14 4:26 AM
Hi, I am using the Keil MCBSTM32f400 evaluation board and currently experimenting with the USB HID example code provided by ST. This code is configured so that the device is self powered rather than bus powered.
I am seeing the following observations. 1) The voltage on PA9(VBUS pin) is ~2.2V on the evaluation board even when no USB cable from the host is connected. 2) When the USB cable from the host is connected, the voltage jumps to ~5V. 3) When the cable is disconnected, the voltage falls back to ~2.2V. As a consequence of this, since the voltage does not fall below 0.8V (per datasheet), the USB session end interrupt is not triggered. Additionally, the USB session request interrupt is fired even when no USB connection is detected (as the default voltage is ~2.2V). the VBUS pin is configured as follows GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOA, &GPIO_InitStructure); Also, NOVBUSSENS bit is reset and VBUSBSEN bit is set in OTG_FS_GCCFG register. I am not seeing any issues with the code. Is there anything i am missing ? Any idea why 2.2V is seen even if there is no USB cable connected ? #usb-vbus #usb-vbus2014-08-14 5:21 PM
> Any idea why 2.2V is seen even if there is no USB cable connected ?
It is caused by the TVS diode array (IC5 and IC8: USBLC6-4). When USB cable is disconnected, VBUS_FS (VBUS_HS) is still pulled up by D+ line, passing through high-side protection diode in this chip, on self-powered configuration. For temporary workaround, a) lift up or cut off pin 6 (VBUS) of this chip or b) remove this part entirely from the board USBLC6-4 datasheet http://www.st.com/web/en/resource/technical/document/datasheet/CD00047494.pdf USBLC6-4 and USBLC6-2 are wrong options for USB Device protection. These parts are good for Host downstream port protection, but never use them for Device upstream port protection. I have warned to Keil on this issue, http://www.keil.com/forum/24795/usb1-vbus-sensing-with-mcb4357/ For USB Device protection, TVS array chip just with low-side diodes is applied. For example, ST ESDAULC6-3BP6 http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/CD00165276.pdf ON Semi NUP4060AXV6 (for full-/low-speed) http://www.onsemi.com/pub_link/Collateral/NUP4060AXV6-D.PDF Tsuneo
2014-09-05 2:31 AM
Hi chinzei.tsuneo,
Your suggestion was most helpful. We removed the IC suggested by you and now the voltage falls to ~0V. Thanks a lot. Vasanth2015-05-07 2:06 AM
Hi chinzei.tsuneo,
Thank you very much for the suggestion. By doing that change, VBus voltage is getting reduced. But i am not getting the UsbDisconnect Interrupt all the times. Some times it is coming and majority of the times it hangs. Can you please help? Regards, Raghavendra GWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.