2011-09-11 6:04 AM
After I've installed the VCP driver and connected USB to the board I get an error in device manager:
''This device cannot start(code 10)'' but when using Windows XP no error occures .. Any idea on how to fix it is welcomed #code-10 #virtual-com #vcp-win7 #stm32f4112011-09-12 11:16 PM
Found the problem, the VIRTUAL_COM_PORT_DATA_SIZE should be 64
and I've used 255 that works on XP but not on Win72011-11-17 12:51 AM
Hi. How do you set the virtual com port data size???
2011-11-17 7:29 AM
2015-05-05 1:45 PM
2015-05-05 5:49 PM
This thread is from *2011*, neither the F411 nor Cube existed in that universe.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.