STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIN BUS non blocking HAL_LIN_SendBreak?

Hi, HAL_LIN_SendBreak seems to be blocking CPU, is there a way to bring UART TX pin down then wait for timer and bring it up? I have done it making GPIO pin GPIO_MODE_OUTPUT_PP then back to GPIO_MODE_AF_PP but init after takes long time. I was wonder...

JBond.1 by Senior II
  • 461 Views
  • 2 replies
  • 0 kudos

Resolved! UART output data gets corrupted

So here is the outline of my code. I'm getting data every 5 seconds (example data: "vref:2975.12, voltage_max:30.00, voltage_min:-1219.00,avg_error: 4136.04") via UART and i transmit it again to view it in putty via ST Link (USART3). Problem is some ...

sreyas40_0-1768217556423.png

Implement WebSocket Protocol on STM32?

Hello,I am currently working on a project with an HTTP server, successfully implemented using FreeRTOS. In this setup, I handle client requests for opening and collecting data from the client side. However, since I need to display real-time data on a...

AS5 by Associate II
  • 6145 Views
  • 11 replies
  • 4 kudos

Resolved! USBD_CDC_ACM_Activate() never get called

Hi,I have implemented CDC USB device on my custom board using STM32C071CBT6. When i connect USB cable to host PC then I can see Virtual COM Port on PC as 'USB Serial Device (COMxx)' However, I tried transmitting some data which I could not receive on...

PPate.1 by Associate III
  • 1604 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H743 Timers + ADC + DMA

Hi you all,as a breef summary; I set up a timer to trigger an adc that should than use the DMA to transfer the data to memory, i need 111 samples at a time. Sadly for some reason this only works for one sample so if i check  __HAL_DMA_GET_COUNTER(g_h...

ICT_TAN_0-1768226675241.png ICT_TAN_1-1768226694036.png ICT_TAN_2-1768226722687.png
ICT_TAN by Associate
  • 514 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.