2026-01-11 5:24 PM - last edited on 2026-01-12 12:05 AM by Gyessine
Dear @YutinhLin ,
Post Edited by ST moderator to apply source code formatting and translate from Chinese to English to comply with the community rule:
Best regards,
Gyessine
晶片型號 : STM32H723VGTx
RX 與 TX Buffer 都已配置到 D2 區塊
使用狀況 :
第一次執行 HAL_UART_Transmit_DMA 正常
執行 HAL_UART_AbortReceive() -> HAL_UARTEx_ReceiveToIdle_DMA() 後
再執行 HAL_UART_Transmit_DMA 無法正常工作
請問這樣的使用方式是否正確
或是需要另外的設定動作才能再正常使用
Chip model: STM32H723VGTx
Both the RX and TX buffers are allocated in the D2 domain.
Usage scenario:
The first execution of HAL_UART_Transmit_DMA operates correctly.
After executing HAL_UART_AbortReceive() followed by HAL_UARTEx_ReceiveToIdle_DMA(), subsequent execution of HAL_UART_Transmit_DMA does not function as expected.
2026-01-12 2:18 AM
Hello @YutinhLin
Can you provide more details about your case. Expected behavior, current behavior, IOC config, your code?
You can see How to write your question to maximize your chances to find a solution for best results.
Also: How to insert source code
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-12 2:24 AM
Hello @YutinhLin
What is the issue exactly that you are encountering? What is the return value of HAL_UART_Transmit_DMA?
2026-01-12 5:05 PM
我想要達到的程式效果是
DMA receive buffer index 每次接收都可從 0 開始
因此會一直去 reset DMA 設定
modbus_send_package 最後的 HAL_UART_Transmit_DMA function 內錯誤點
void CO_DMA_CRL(FunctionalState state)
{
if(state==DISABLE)
{
if(HAL_OK==HAL_UART_AbortReceive(CO_INFO.channel))
CO_INFO.dma_status=DISABLE;
}
else
{
CO_INFO.RX.data = (uint8_t *)co_dma_rx_data;
if(HAL_OK==HAL_UARTEx_ReceiveToIdle_DMA(CO_INFO.channel,(uint8_t*)CO_INFO.RX.data,CO_UART_BUF_LENGTH))
CO_INFO.dma_status=ENABLE;
}
}
void modbus_send_package(uint8_t dev_addr, uint8_t fun_id, uint8_t reg, uint16_t reg_count, uint16_t *send_data)
{
uint16_t crc=0;
uint16_t data_tmp;
uint8_t send_len=0;
CO_INFO.send_func_id = fun_id;
CO_INFO.read_start_reg = reg;
CO_INFO.read_reg_count = reg_count;
CO_INFO.send_data = send_data[0];
co_dma_tx_data[0]=dev_addr;
co_dma_tx_data[1]=fun_id;
if(fun_id == MODBUS_FUN_ID_READ_INFO)//read holding register
{
co_dma_tx_data[2]=(reg>>8)&0xFF; //start register address High byte
co_dma_tx_data[3]=reg&0xFF; //start register address Low byte
co_dma_tx_data[4]=(reg_count>>8)&0xFF; //register read count High byte
co_dma_tx_data[5]=reg_count&0xFF; //register read count Low byte
crc=MODBUS_CRC16(co_dma_tx_data,6);
co_dma_tx_data[6]=(crc>>8)&0xFF; //crc Low byte
co_dma_tx_data[7]=crc&0xFF; //crc High byte
send_len=8;
}
else if(fun_id == MODBUS_FUN_ID_WRITE_SINGLE) //write single register
{
co_dma_tx_data[2]=(reg>>8)&0xFF; //register address High byte
co_dma_tx_data[3]=reg&0xFF; //register address Low byte
data_tmp=send_data[0];
co_dma_tx_data[4]=(data_tmp>>8)&0xFF; //write data High byte
co_dma_tx_data[5]=data_tmp&0xFF; //write data Low byte
crc=MODBUS_CRC16(co_dma_tx_data,6);
co_dma_tx_data[6]=(crc>>8)&0xFF; //crc Low byte
co_dma_tx_data[7]=crc&0xFF; //crc High byte
send_len=8;
}
else if(fun_id == MODBUS_FUN_ID_WRITE_MULTI) //write multiple register
{
co_dma_tx_data[2]=(reg>>8)&0xFF; //start register address High byte
co_dma_tx_data[3]=reg&0xFF; //start register address Low byte
co_dma_tx_data[4]=(reg_count>>8)&0xFF; //register write count High byte
co_dma_tx_data[5]=reg_count&0xFF; //register write count Low byte
co_dma_tx_data[6]=reg_count*2; //byte count
for(uint16_t i=0;i<reg_count;i++)
{
data_tmp=send_data[i];
co_dma_tx_data[7+i*2]=(data_tmp>>8)&0xFF; //write data High byte
co_dma_tx_data[8+i*2]=data_tmp&0xFF; //write data Low byte
}
crc=MODBUS_CRC16(co_dma_tx_data,7+reg_count*2);
co_dma_tx_data[7+reg_count*2]=(crc>>8)&0xFF; //crc Low byte
co_dma_tx_data[8+reg_count*2]=crc&0xFF; //crc High byte
send_len=9+reg_count*2;
}
else
{
CO_INFO.send_func_id=0;
CO_INFO.read_start_reg=0;
CO_INFO.read_reg_count=0;
CO_INFO.send_data = 0;
return;
}
if(HAL_OK != HAL_UART_Transmit_DMA(CO_INFO.channel, co_dma_tx_data, send_len))
{
DEBUG_PRINT("CO MODULE SEND DATA ERROR!!\r\n");
}
}
2026-01-12 5:05 PM
HAL_UART_Transmit_DMA function 內錯誤點
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.