2026-01-03 1:54 AM
Hi, HAL_LIN_SendBreak seems to be blocking CPU, is there a way to bring UART TX pin down then wait for timer and bring it up? I have done it making GPIO pin GPIO_MODE_OUTPUT_PP then back to GPIO_MODE_AF_PP but init after takes long time. I was wondering is it possible to do it within UART without changing pin mode? Or reducing the time pin mode init is required?
void LIN_SendFrame_IT(void)
{
__HAL_UART_DISABLE(&huart2);
GPIO_InitTypeDef g = {0};
g.Pin = LIN_TX_Pin;
g.Mode = GPIO_MODE_OUTPUT_PP;
g.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(LIN_TX_GPIO_Port, &g);
HAL_GPIO_WritePin(LIN_TX_GPIO_Port, LIN_TX_Pin, GPIO_PIN_RESET);
TIM2->ARR = 900; // 900us break
TIM2->CNT = 0;
TIM2->CR1 |= TIM_CR1_OPM;
HAL_TIM_Base_Start_IT(&htim2);
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim != &htim2) return;
HAL_GPIO_WritePin(LIN_TX_GPIO_Port, LIN_TX_Pin, GPIO_PIN_SET);
GPIO_InitTypeDef g = {0};
g.Pin = LIN_TX_Pin;
g.Mode = GPIO_MODE_AF_PP;
// This takes way too long to retunt to UART
HAL_GPIO_Init(LIN_TX_GPIO_Port, &g);
__HAL_UART_ENABLE(&huart2);
HAL_UART_Transmit_DMA(&huart2, &DATA, 1); //Transmit
}
Solved! Go to Solution.
2026-01-03 2:01 AM - edited 2026-01-03 2:02 AM
@JBond.1 wrote:HAL_LIN_SendBreak seems to be blocking CPU
What makes you say that?
The source doesn't seem to suggest it:
/**
* @brief Transmits break characters.
* @PAram huart Pointer to a UART_HandleTypeDef structure that contains
* the configuration information for the specified UART module.
* @retval HAL status
*/
HAL_StatusTypeDef HAL_LIN_SendBreak(UART_HandleTypeDef *huart)
{
/* Check the parameters */
assert_param(IS_UART_INSTANCE(huart->Instance));
/* Process Locked */
__HAL_LOCK(huart);
huart->gState = HAL_UART_STATE_BUSY;
/* Send break characters */
ATOMIC_SET_BIT(huart->Instance->CR1, USART_CR1_SBK);
huart->gState = HAL_UART_STATE_READY;
/* Process Unlocked */
__HAL_UNLOCK(huart);
return HAL_OK;
}
2026-01-03 2:01 AM - edited 2026-01-03 2:02 AM
@JBond.1 wrote:HAL_LIN_SendBreak seems to be blocking CPU
What makes you say that?
The source doesn't seem to suggest it:
/**
* @brief Transmits break characters.
* @PAram huart Pointer to a UART_HandleTypeDef structure that contains
* the configuration information for the specified UART module.
* @retval HAL status
*/
HAL_StatusTypeDef HAL_LIN_SendBreak(UART_HandleTypeDef *huart)
{
/* Check the parameters */
assert_param(IS_UART_INSTANCE(huart->Instance));
/* Process Locked */
__HAL_LOCK(huart);
huart->gState = HAL_UART_STATE_BUSY;
/* Send break characters */
ATOMIC_SET_BIT(huart->Instance->CR1, USART_CR1_SBK);
huart->gState = HAL_UART_STATE_READY;
/* Process Unlocked */
__HAL_UNLOCK(huart);
return HAL_OK;
}
2026-01-14 8:51 AM
Seems to be my bad, looks like its not blocking, which is ok, just maybe wanted longer pause at start than 13 bits
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.