STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB PD change voltage during active contract

Dear ST Community, I have a working application for USB PD SPR and EPR and now I want to change the voltage (power profile) during an active contract.So e.g. I have 5V currently and want to request 9V from the source, or I have 20V currently and want...

abtq by Associate III
  • 1268 Views
  • 8 replies
  • 2 kudos

Resolved! Output gain set is omitted in WM8904_Init()

Hi,// WM8904.c int32_t WM8904_Init(WM8904_Object_t *pObj, WM8904_Init_t *pInit) // ... if ((WM8904_CurrentDevices & WM8904_OUT_HEADPHONE) == WM8904_OUT_HEADPHONE) { ret += WM8904_SetVolume(pObj, VOLUME_OUTPUT, (uint8_t)pInit->Volume); } ...

ERROR by Senior
  • 285 Views
  • 2 replies
  • 1 kudos

Writing to flash generates a HardFault

Hi,I'm busy with my own BootLoader. I can erase the flash, required to store the program. But writing to the flash causes a HardFault. (I also write to flash in my application to store the configuration. That seems to work, so (normally) I can write ...

ErX_0-1769163253275.png ErX_1-1769163274310.png
ErX by Associate III
  • 417 Views
  • 4 replies
  • 1 kudos

Noekeon MCE not working on OSPI

Hello, i'm trying to using mce encription for external flash. I have the stm32h7s7-dk eval board.my mce configuration for the external memory init; my mce configuration for the boot main I followed the tutorial series https://www.youtube.com/watch?v=...

Screenshot from 2026-01-22 16-20-54.png Screenshot from 2026-01-22 16-21-24.png Screenshot from 2026-01-22 16-25-32.png Screenshot from 2026-01-22 16-25-41.png
neset by Associate II
  • 238 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.