STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Data Transfer with STM32L552E-EV

Greetings,Kindly, I would like to know which USB interface I can use to transfer data between the STM32L552E-EV and the reComputer J4012.I am working with TEE, and my goal is to send plaintext from the reComputer to the STM32L5 so that it can be encr...

Nirene by Associate II
  • 749 Views
  • 8 replies
  • 5 kudos

Resolved! Ethernet Lwip Ping

Hi, I want to set up the Ethernet peripheral of the STM32H743 microcontroller using lwIP, but I’m facing a problem and I can’t get a ping response. I have reviewed some codes, but they don’t fully explain the cause of the issue. Does anyone have expe...

Example for USB HID / NUCLEO-071RB

I have a NUCLEO-071RB development board.Is there a ready to run example for this board somewhere?I tried to generate a bare bone example with CubeMX.The code loads and runs but hangs in here:MX_ThreadX_Init =>  tx_kernel_enter => tx_initiali ze_kerne...

nyholku by Associate
  • 216 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.