STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Help with confguring STM32H7

CubeIDE: v2.0.0CubeMX: v6.16.1Debugger: ST-LINK/V2 V2J46S7Hello,I'm attempting to setup a dual core project using STM32H757XIH MCU on CubeMX. I've generated and imported the project for CubeIDE. I've configured the Trace and Debug -> DEBUG for "Seria...

schradz by Associate II
  • 320 Views
  • 4 replies
  • 0 kudos

STM32G491 and BOOT_LOCK

STM32G491KEU3 on custom board. Using STM32CubeProgrammer to read/change option bytes.With BOOT_LOCK unchecked I use STM32CubeIDE to flash and debug my project. However SysTick_Handler() is never called, so HAL_GetTick() always returns the same value ...

STM32U5A9 USB MSC

  We are currently working on a project with the STM32U5 series running FreeRTOS and need to integrate the USB Mass Storage (MSC) class for adding pendrive / thumbdrive support. While exploring solutions, we noticed that CubeIDE doesn't directly supp...

nfkt by Associate
  • 1008 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 H264 video encoder and streaming over RTSP

Hello, I would like to know the H264 VENC performance for the STM32N6 using the ST example: STM32Cube_FW_N6_V1.1.1/Projects/STM32N6570-DK/Applications/VENC/VENC_RTSP_ServerI have a hardware setup with a nucleo-n657x0-q + a ST B-CAMS-IMX camera module...

FB__1 by Associate III
  • 2581 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.