2025-12-31 8:47 AM - last edited on 2026-01-19 2:04 AM by Saket_Om
I'm trying to develop a basic PDM microphone to PCM audio data application on the NUCLEO-U575ZI-Q development board. I have tried to adapt the ADF_AudioRecorder application designed for the STM32U575I-EV and found at https://github.com/STMicroelectronics/STM32CubeU5/tree/5107fbd316d605704bb4c3ebf2126d4d1ba0e763/Projects/STM32U575I-EV/Examples/MDF/ADF_AudioRecorder
I can generate the ADF CCK0 clock output on PE09 (confirmed 1.01 MHz with my oscilloscope) and when connected to my PDM microphone, see the PDM output on its DATA line, also using my oscilloscope, and connect this to PE10.
Because I have no SAI and no audio CODEC attached, I just want to save the PCM formatted samples to memory at the moment, with a view to exporting over the VCOM port for verification in future. However, I'm stuck at the point of creating the samples. From the .ioc file attached, you should be able to see my configuration is, aside from the SAI, very similar to the example for the other U5 dev board. I am setting volatile flag variables in the DMA complete/half-complete interrupt callbacks in the user code section but neither appear to be triggering as my LED is staying either fully off or fully on (depending on whether I turn it on or off prior to entering my while{} loop). Verified by also probing LED with oscilloscope to confirm I'm not suffering a persistence of vision illusion.
GPDMA channel 11 interrupt is set up as far as I can tell and I'm successfully calling `HAL_MDF_AcqStart_DMA()`
@coppercrimp seemed to have some success in the past with this kind of application so I humbly ask if they would mind commenting (what extra info would be useful?), as well as ST staff and wider community.
2026-01-19 2:23 AM
Hello @Simon_M
I recommend temporarily toggling a LED in the IRQ handler itself:
void GPDMA1_Channel11_IRQHandler(void)
{
HAL_GPIO_TogglePin(LED_GREEN_GPIO_Port, LED_GREEN_PIN); // quick visual check
HAL_DMA_IRQHandler(&handle_GPDMA1_Channel11);
}
If this never toggles, the DMA is not generating any interrupts (no transfer started, wrong request).
If it toggles, you should check which specific interrupt flag is actually triggering the IRQ.
2026-01-22 12:59 PM
Thank you for your suggestion. I added an LED toggle to the IRQ handler:
void GPDMA1_Channel11_IRQHandler(void)
{
/* USER CODE BEGIN GPDMA1_Channel11_IRQn 0 */
HAL_GPIO_TogglePin(LED1_GPIO_PORT, LED1_PIN); // quick visual check LED_GREEN
/* USER CODE END GPDMA1_Channel11_IRQn 0 */
HAL_DMA_IRQHandler(&handle_GPDMA1_Channel11);
/* USER CODE BEGIN GPDMA1_Channel11_IRQn 1 */
/* USER CODE END GPDMA1_Channel11_IRQn 1 */
}But this made no difference. Can you suggest something else please?
2026-01-22 1:51 PM
PS, we have the example working on NUCLEO-U545RE, just can't get it working on the U575 now which is very strange. We can't tell what the difference would be. What do you think it will be? We have triple-checked pinout etc. And yes, we need it working on the U575.
2026-01-23 1:07 AM
Hello @Simon_M
Could you try with the same MDF_DMAConfig as in the example.
static void MDF_DMAConfig(void)
{
/* Initialize DMA configuration parameters */
DMAConfig.Address = (uint32_t)&RecBuff[0];
DMAConfig.DataLength = (REC_BUFF_SIZE * 4U);
DMAConfig.MsbOnly = ENABLE;
}
In your code you are configuring MsbOnly to DISABLE.
2026-01-23 2:43 AM
It's a good thought, thank you, but I incidentally tried
DMAConfig.MsbOnly = ENABLE;
yesterday when comparing the example to my version. It was unsuccessful unfortunately. The only other area I can see that slightly differs is the clock settings (PLL is not used, just MSIK in my version) but I don't know if this can really be an area of suspicion as the ADF output clock is definitely present (both clock to PDM mic and data from PDM mic are verified on oscilloscope as present to suitable frequency and voltage levels).
What should be my next priority to do?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.