STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FLASH programming issue on HAL_FLASH_Unlock

Hi there!I'm experiencing a new trouble: trying to program a simple flash Word it results in an hard fault; moreover, also trying to read the same area gives an hard fault.Debugging the application I discovered that the HAL_FLASH_Unlock function fail...

iTTy by Senior
  • 3727 Views
  • 2 replies
  • 0 kudos

Resolved! FFT function and buffer size

Watching some videos online about FFT and trying to use (in STM32CubeIDE) the arm_rfft_fast_f32 function of the arm_math.h DSP library, it is not clear to me why the buffer output produced by that function is N/2 long and not NIs it something related...

luke514_0-1706189998758.png
luke514 by Senior
  • 2219 Views
  • 1 replies
  • 1 kudos

ALTCP causes LAN7820 link detection to fail

Working with STM32H743IIT single CM7 core MCU I was managed to have a stable product with Ethernet connectivity. Thanks everybody (@Piranha especially) for your advicesNow I was going to implement secure communication over ALTCP instead of regular ma...

ktrofimo by Senior III
  • 1363 Views
  • 0 replies
  • 0 kudos

Micro SD whith micro controller

Good morning,This is my first postI' m searching for a special micro SD card with:• MCU: 32-bit (produced by ST)• MCU clock: > 100MHz• RAM: > 384 Kbytes• Flash: > 768 Kbytes• Timer function• Random number generator function• Secure memory area requir...

FuscoV by Associate
  • 1774 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0B1 USB fails to request device descriptor

Hi, I'm running into problems registering USB interfaces on STM32G0B1KBU6.  The same code works fine on STM32F1*, STM32F7*, and STM32G4*.Environment: latest STM32CubeIDE (v.1.13.2) @ Windows.  Target: custom board with STM32G0B1KBU6, which uses the f...

romp by Associate II
  • 2255 Views
  • 1 replies
  • 0 kudos

Resolved! q1.15 Format

I have 1024 integer numbers in an array that are between 0 and 4096. Now I'm trying to convert these array values to Q1.15 format. These should then be between -1 and +1. With my attempt, I don't achieve any negative values, all of them are just posi...

Sax by Associate III
  • 1910 Views
  • 1 replies
  • 1 kudos

Resolved! USB CDC example for STM32F072 (Disco board)

I bought an STM32F072 disco board specifically to develop a USB CDC application, but I can't now find an example or demo in STM32CubeMX V6.10. I found this thread https://community.st.com/t5/stm32-mcus-products/stm32f070-usb-cdc-example/m-p/457994#M1...

Hal_Gettick() always returns 0 for STM32F0 DISCOVERY

Hi, I am working on custom Bootloader and Application stored with different starting address on same Flash When I jump from my Bootloader to Application area which contains Blinking LED With HAL_Delay() function  my application is stuck in HAL_Delay ...

VBAS by Associate
  • 1550 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.