2024-01-23 3:24 AM
I have 1024 integer numbers in an array that are between 0 and 4096. Now I'm trying to convert these array values to Q1.15 format. These should then be between -1 and +1. With my attempt, I don't achieve any negative values, all of them are just positive. Thanks for the help.
float32_t fir_in_arm [1024],fir_out_arm [1024],fir_state [1089-1];
int16_t fir_in_temp [1024]; // with float32_t also tried and no success
float32_t fir_in_temp_gleit [1024];
for (int i = 0; i<= adcBufferSize; i++)
{
adc_buffer_float[i] = (float32_t)adc_buffer [i];
fir_in_temp_gleit[i] = (adc_buffer_float[i])/32767;
fir_in_temp [i] = fir_in_temp_gleit[i]*32768;
}
Solved! Go to Solution.
2024-01-23 4:38 PM - edited 2024-01-23 4:38 PM
To map (0, 4096) to q1.15 (expressed as an int16_t):
uint16_t input = 0 ... 4095;
float mid = input / 2048.0f - 1.0f;
int16_t output = (int16_t) (mid * 32768);
Or all in one statement:
int16_t output = (int16_t) ((input / 2048.0f - 1.0f) * 32768);
Gives the following mapping:
0 -> -1.000 -> -32768
256 -> -0.875 -> -28672
512 -> -0.750 -> -24576
768 -> -0.625 -> -20480
1024 -> -0.500 -> -16384
1280 -> -0.375 -> -12288
1536 -> -0.250 -> -8192
1792 -> -0.125 -> -4096
2048 -> 0.000 -> 0
2304 -> 0.125 -> 4096
2560 -> 0.250 -> 8192
2816 -> 0.375 -> 12288
3072 -> 0.500 -> 16384
3328 -> 0.625 -> 20480
3584 -> 0.750 -> 24576
3840 -> 0.875 -> 28672
2024-01-23 4:38 PM - edited 2024-01-23 4:38 PM
To map (0, 4096) to q1.15 (expressed as an int16_t):
uint16_t input = 0 ... 4095;
float mid = input / 2048.0f - 1.0f;
int16_t output = (int16_t) (mid * 32768);
Or all in one statement:
int16_t output = (int16_t) ((input / 2048.0f - 1.0f) * 32768);
Gives the following mapping:
0 -> -1.000 -> -32768
256 -> -0.875 -> -28672
512 -> -0.750 -> -24576
768 -> -0.625 -> -20480
1024 -> -0.500 -> -16384
1280 -> -0.375 -> -12288
1536 -> -0.250 -> -8192
1792 -> -0.125 -> -4096
2048 -> 0.000 -> 0
2304 -> 0.125 -> 4096
2560 -> 0.250 -> 8192
2816 -> 0.375 -> 12288
3072 -> 0.500 -> 16384
3328 -> 0.625 -> 20480
3584 -> 0.750 -> 24576
3840 -> 0.875 -> 28672
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.