STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Strange internal FLASH reading after sector erase.

Hi there!Experimenting FLASH reading/writing I done a fanny test that is giving an unexpected (to me) result.Basically:1) I defined  2 32 bytes buffers (aRbuff for read, and aWbuff for write) u32t aWbuff[8U] = { 0x00010203, 0x04050607, 0x08090A0B, ...

iTTy_0-1706202595688.png
iTTy by Senior
  • 5506 Views
  • 9 replies
  • 5 kudos

STM32F407 + CGI Handler

 Hello everyone,I am using the STM32F407 µC and would like to create a web interface. A few functions, such as getting the temperature value from the µC once (SSI) and switching on the LED via the web interface on the board (CGI), work. Now I would l...

Ina_0-1706269581280.png Ina_2-1706269658737.png Ina_1-1706269637603.png
Ina by Associate
  • 1470 Views
  • 1 replies
  • 0 kudos

Resolved! bare-metal core testing for STM32G0

Hi, I need 60370 class-B certification, but without incorporating libraries that we cannot check ourselves. So, I rather develop bare-metal tests than dropping the X-CUBE-CLASSB object into the code. Testing the Cortex-M0 core should be possible with...

About stm32 usb uvc data transmission

sir, Hope you doing all are well.......Presently am working on Stm32f746ZG NUCLEO board. am working on usb uvc communication between MCU and computer.so i need to send image/video data on usb using uvc protocol.I got some developed code from le...

steja by Associate II
  • 4090 Views
  • 2 replies
  • 2 kudos

Any example on STM32F2xx with UVC?

Posted on June 03, 2012 at 13:59Hi, Does anybody know if there is example on STM32F2xx to support UVC class? I checked USB lib provided by STM but only similar example (Audio with ISO out) provided and I do think there should be quite some works if...

USB device with stm32u59

I would like to get started with simple usb device detection and read/write operation , From what i can see , the usb library support is limited to the stm32u5x, my application use freertos but all documentaion i find is regarding USBX and no other u...

Anassoumi by Associate III
  • 1027 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.