2024-01-24 2:37 AM
Good morning,
This is my first post
I' m searching for a special micro SD card with:
• MCU: 32-bit (produced by ST)
• MCU clock: > 100MHz
• RAM: > 384 Kbytes
• Flash: > 768 Kbytes
• Timer function
• Random number generator function
• Secure memory area required to store encryption keys
• Flash of at least 8Gb
• Sdk to develop and Upload software on microcontroller (ex: rsa and AES key generation function)
• Password or PIN for data protection stored on the flash (not for read but only for mofify/delete/create)
Is there anyone who can recommend me some manufacturers please?
Thank you
Vincenzo
2024-01-24 3:34 AM - edited 2024-01-24 3:44 AM
Hello @FuscoV and welcome to the ST Community :smiling_face_with_smiling_eyes:.
If you are locking for an STM32 with specific characteristics. I suggest you use the MCU/MPU selector included in CubeMX:
or the ST MCU Finder. Then, using the filters you can make the choice of product.
PS: What this mean "a special micro-SD card with: MCU: 32-bit (produced by ST)"
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-24 3:41 AM - edited 2024-01-24 4:34 AM
But does it have any option for, "an STM32 on a micro-SD Card" ?
:thinking_face:
EDIT: Ah - I see you've added::
@STTwo-32 wrote:PS: What this mean "a special micro-SD card with: MCU: 32-bit (produced by ST)"
I think @FuscoV wants the STM32 embedded within the uSD card?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.