2024-01-20 5:37 PM
Hi, I am working on custom Bootloader and Application stored with different starting address on same Flash
When I jump from my Bootloader to Application area which contains Blinking LED With HAL_Delay() function my application is stuck in HAL_Delay ()function.And also I have observed that if I debug using break points it is executing perfectly, but not working in run mode.
Can anyone please help
Thanks in advance
2024-01-23 4:54 AM
Hello @VBAS ,
If your application gets stuck in the HAL_Delay() function, it might be due to the system clock not being properly configured. Make sure the system clock is correctly initialized in your application.
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.