STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LT8491

HOW to interface LT8491 BUCK boost converter module  with STM32F103RCt6tr board with i2c protocol and give detailed explanation and if posiible give an example code

Resolved! RM0444 bus stall while program/erase Flash memory.

Hello,i have a question regarding the RM0444. On page 74  chapter 3.3.6, is mentioned the following:"During a program/erase operation to the Flash memory, any attempt to read the Flashmemory stalls the bus. The read operation proceeds correctly once ...

che747 by Associate
  • 2290 Views
  • 2 replies
  • 1 kudos

USB OTG dual role - auto switch over - configuring

Hello,We are using a STM32F407 discovery board. We need to configure the USB as OTG/Dual_Role_Device. I have each (USB Host and USB Device) working in separate projectsIn CubeMX when I select OTG/Dual_Role_Device, the USB_DEVICE and USB_HOST are gray...

BAW by Associate III
  • 3562 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F407 to STM32F407 USB communications

Hello,I am new to STM32 parts and USB. We are looking at using USB to communicate between two STM32F407 boards.Can anyone give some insight as to the best way to do this?What USB classes should be used?Any examples of this?Thanks,Brent

BAW by Associate III
  • 3499 Views
  • 5 replies
  • 1 kudos

CIMSIS 5.9 (Source) - missing dependencies

Hello Community!I just started a new project and wanted to use CMSIS 5.9 - as it finally can be installed from the package without errors.Until now I only used CMSIS 5.7 als library, which worked pretty well. Unfortunately since 5.9 there is no libra...

a4.png a3.png a1.png a2.png
CBerg by Senior II
  • 2584 Views
  • 2 replies
  • 3 kudos

SDIO Error when use SD NAND chip

I have been using microSD chips reliably for many years with stm32f4, stm32h7 and stm32l4.But for one of my products, where space is at a premium, I am trying to use a SD-NAND chip XTSD04G, and I am running into occasional errors where an SDIO R1 com...

Danish1 by Lead III
  • 1949 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.