Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, I am trying to acquire a signal connected to PC0 with ADC using an STM32L486RG. I used this code with a nucleo evaluation board and it works fine but when i move to the PCB the voltages read by the mcu are really low. The signal in the PCB oscill...
My target is STM32F103C8T6. My project works when I generate a .bin file and upload it using the stand-alone st-link utility configured as "connect under reset". I cannot upload directly from the IDE, I get the errors:--------------------------------...
Hi All,By default, we can easily program the evaluation board by dragging the .bin file into the Mass Storage Device of the evaluation board.Unfortunately, my company has restricted the mass storage class. Therefore there is no way I can program the ...
Hi, my mcu is not showing up in st-link v2 :( Currently boot0 i low, 10k resistor to gnd. All voltages are stable on vdd and no short circuit is detected. Any tips or possible solutions to my problem?My schematic can be found here: https://gyazo.com/...
Recently I've bought two isolated probes (from mouser). After attaching them to the target I've discovered that both consumes approx. 500 uA (measures with fluke multimeter). But I'm also have older stlink/v2 isol which I used earlier, and it hasn't ...
i connected st link to my stm32 on customboard , 1 pin -> 3.3V, 7 pin -> SWDIO, 9 pin -> SWCLK, 15 pin-> NRST, 19 pin -> GND. but keil doesn't recognize mcu. I attach the image of the connection . st link was damaged or wrong pin configuration? thank...
Hi. I have been using MCU STM32F407ZET6.But I don't know how to connect PDR_ON pin exactly.Nowadays there are some errors about this chip on board.I saw your document named AN4488.But I still don't know how to make a schematic about PDR_ON pin.Could ...
They have given male connecting headers, I need the extension connecting headers to connect with other modules using the communication protocols.
https://www.st.com/en/evaluation-tools/stm32f4discovery.html#resourceit seems only the pdf files are still available
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.