Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, I update my STlinkv2 from V2J29M18 to V2J34M25 firmware version and i lost the UART communication.I have two STlinkV2 and one is always in V2J29M18 version so i'm sure that the problem come from the update.So my question is how i can restore the ...
I use ST-Link/V2 with ST-LINK_CLI.exe to program my firmware into a STM32L452. The command I use is: ST-LINK_CLI.exe -P Myfile.hex -V -RstProgramming works fine, no error. But at the end I’m expecting my firmware to start running automatically and as...
Hi All,I am using STM32L071KZ in my application. In my design I made the controller to program via UART2.When I connected St Link V3 to my PC its showing only Following mode to program:JTAG, SWD, SPI, I2C and CAN but not UART.To know more please see ...
Hi, I have downloaded ST-LINK driver application from STM website. But it cannot be installed in my 64bit Windows10 laptop. When I run the application dpinst_amd64, it says cannot complete the device driver installation wizard. Please see the attachm...
Hi,I would like to know if there is any pdf with more information about the board than what can be found on:DB3741 (data brief)MB1381 (Schematics)I expected to get a more detailed description of the board and its usage.Thank you
Just got my STM32H745 DISCO today. I notice ST uses ST-Link V3 on all dual core boards. Does ST-Link V2 still work for dual core lines? I searched around on ST website and could not find any answers. Beers provided for anyone giving a hint ;)
Hello I’m using a STM32L4R9I Discovery board at the moment and want to have some documentation besides the demo code about the MFX µC on the board wich is in charge of e.g. the joystick and the power measurement. In the User manual for the discovery ...
We are using STM32L151VCT6A MCU. I have already programmed and worked on the boards, but for 2nd time device is not allowing to read/write the program. And even the pin numb 72 is low at the MCU.
I had my C code running on NUCLEO-F411RE last week. I downloaded it with Keil uVision and STLink driver. But, I did something when I tried to flash it today with an assembly code instead of the C code. Now, I cannot flash the device.* A pop up win...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.