STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745I-Disco board: how to flash extra QSPI flash with ST-LINK V3SET when debug?

I have a new problem for flash extra QSPI flash chip MT25QL512 in STM32H745I-Disco board with IAR v8.11.  When debug, the following is the information:Sun Jun 16, 2019 20:24:50: Flash download warning: 327424 out of 327424 bytes from data record CODE...

0690X000008ikcKQAQ.png
YWu.19 by Associate II
  • 3163 Views
  • 6 replies
  • 1 kudos

Is my circuit for building a MC board fine?

Hi guys, I have built this STM32F334K4T6 MC dev board, I want to know if the schematic and the PCB wiring are all fine. I also would want to know if the board will power on and will I be able to upload code to it and see an LED blink or so. I have at...

Sashvat by Associate II
  • 12200 Views
  • 23 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.