2019-06-02 12:27 PM
My target is STM32F103C8T6. My project works when I generate a .bin file and upload it using the stand-alone st-link utility configured as "connect under reset". I cannot upload directly from the IDE, I get the errors:
-----------------------------------------
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
--------------------------------------------------
Any tutorials on how to configure st-link in STM32CubeIDE?
Thank you!
2019-06-08 12:40 AM
I am also looking for an answer on this topic. Were you able to successfully perform Debug using ST-LINK GDB SERVER?
I'm also getting the above error. Please let me know you are able to program the target through STM32CUBEIDE?
2019-06-10 3:35 PM
I never found a way so have been using an external utility.
2019-06-24 6:14 AM
I have a sample problem.
I'm using NUCLEO-F103RB with STM32CubeIDE V1.0.1
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.