STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G031 Discovery and Keil uVision

Hi there!i buy a STM32G031 Discovery Kit, i try to program with Keil uVison but gave me this error "No target connected" , i download the last version USB driver for STLINK but i have the same problem. Some one can help me ?Thank you Sergio

SGian.1 by Senior
  • 2178 Views
  • 7 replies
  • 0 kudos

Resolved! STM32H7XX device security bit error

hiI have a question while set Option byte using STM32 ST-LINK Utility.I'm testing STM32H750 MCU (chip, socket EVK, ST-Link) After I set the Security bit using ST-Link Utility, MCU can't debug anymore. (like figure1)Is it right that setting Security b...

0693W00000D0QgKQAV.png 0693W00000D0QflQAF.png
JCHUN.2 by Associate
  • 1292 Views
  • 1 replies
  • 0 kudos

Resolved! If octospi is enabled system memory is mapped at 0x00 after reset even thought flash should be mapped.

Dear all,I am using a NUCLEO-L4R5ZI board and am trying to get the octospi interface running in quad mode.After generating the code I tried to run the generated code in the STM32CubeIDE but failed to debug it. Since it seems that the system memory ge...

0693W00000D0ILxQAN.png 0693W00000D0ILsQAN.png
Seegras by Associate II
  • 4818 Views
  • 3 replies
  • 0 kudos

What has changed in Cube IDE v1.7?

I have frozen my project on v1.6.1, for good reasons because I don't want new libraries; the existing ones are already massively bloated and full of bugs :)Have they fixed bugs likecannot delete the .elf file (the STLINK debugger is grabbing it - alr...

PHolt.1 by Senior III
  • 1402 Views
  • 2 replies
  • 0 kudos

I am planing to design a USB interface for programming purposes on STM32H743VIT6 as the bootloader is already integrated on the µC.

I wondering on which hardware configuration, I have to implement for this purpose.Could I just use the differential pair as in joined picture without VBUS (as the µC is supplier on Board)?I would like to get more details on how to design this interfa...

SAbis by Associate III
  • 2597 Views
  • 2 replies
  • 0 kudos

Hello, I am designing my Hadrware base on STM32H743VI. Was looking for Power supply application note I could not find any. I would like to know how I would have to connect my VCAP as the LDO is not used or provided. Shall I put it on 100n??

What about Vref+??As I am not using any Battery, I have decided to connect Vbat directly to VDD, is that correct?OSC32 will not be used in my app, will it be possible for to leave it open?

SAbis by Associate III
  • 1302 Views
  • 2 replies
  • 0 kudos

Resolved! ST-Link v3 Mini with STM32CubeIDE

HiI am using STM32CUBEIDE on macOS. Until now I used my ST-Link v2 via SWD with no problems. I have recently upgraded to an ST-Link v3 MINI and implemented the STDC14 connector on my custom pcbs. The pinout is according to the datasheet (the pins on ...

LStoe.1 by Associate II
  • 6313 Views
  • 8 replies
  • 0 kudos

ST-Link implementation on a customer board

I want to copy-paste ST-Link implementation from a Nucleo or Discovery board to my customer board with STM32H7 processor. This way, the board will have one USB connector to use for programming, debugging, upgrading, and finally, for serial communicat...

bigfoot by Associate II
  • 1933 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.