2021-07-04 5:37 AM
Hi
I am using STM32CUBEIDE on macOS. Until now I used my ST-Link v2 via SWD with no problems. I have recently upgraded to an ST-Link v3 MINI and implemented the STDC14 connector on my custom pcbs. The pinout is according to the datasheet (the pins on the ST-Link are numbered and DIO is 4, CLK 6 and so on..)
however: when I open STM32CUBEIDE it recognizes the st-link but when I hit run or debug, it will return "no target found". When I disconnect the ST-Link v3 and connect my st-link v2 I am able to flash the board with no problems.
the ST-Link v3 MINI led is always red during this process.
Does anybody have a clue on how to handle this? I also did not manage to use the drag&drop function...
Solved! Go to Solution.
2021-07-05 7:20 AM
A good point would be to check how does it behave with STM32CubeProgrammer tool. If there are problems detecting STM32 device, it may be linked to wrong pinout. This would eliminate potential issue linked to CubeIDE as mentioned by Markus.
2021-07-05 5:28 AM
Hello there!
A few questions so I can get a better understanding of the issue.
What version of macOS are you using?
We recently found an issue where the first time a launch happens on macOS it can get this error but a second launch works. Any chance it's the same for you?
Are you using the ST-Link GDB Server? Could you send me the gdb server log? You can activate it in your debug configuration.
2021-07-05 7:20 AM
A good point would be to check how does it behave with STM32CubeProgrammer tool. If there are problems detecting STM32 device, it may be linked to wrong pinout. This would eliminate potential issue linked to CubeIDE as mentioned by Markus.
2021-07-06 1:21 AM
Hello,
I have an STLink V3 Mini and it is working fine on a Nucleo G491RE.
You can try If you have a recent Nucleo that have an external 10 pins Debug Connector,
You must set the supply jumper to 5V_charger and set the jumper JP1 to Reset the embedded STLink next to the STLink USB connector.
If you don't have other board to try, you can check what pins are mandatory to connect from the Nucleo's board schematic.
The flat cable is using only the 10 pins in the center for Nucleo. (V3 mini has a 14 pins flat cable).
Rgds,
Laurent
2021-07-06 2:31 AM
Does your target stay long in WFI? StlinkV3 is very bad at connecting to such targets. Did you try to connect under reset (if reset is connected)?
2021-07-17 3:37 AM
How do I check if it stays long in WFI?
I have connect under reset enabled in the debug configuration in STM32CubeIDE
2021-07-17 3:43 AM
with STM32CubeProgrammer I am able to read out the memory.
I click connect, then everything shows up, device name seems correct etc. but after a couple of seconds the ST-Link gets disconnected: macOS gives a warning that I have disconnected the ST-Link without ejecting it and CubeProgrammer says "Warning: Connection to device 0x417 is lost"
This is the log:
12:39:35 : ST-LINK SN : 0015003A3156501620323443
12:39:35 : ST-LINK FW : V3J7M3
12:39:35 : Board : STLINK-V3MINI
12:39:35 : Voltage : 3.44V
12:39:35 : ST-LINK error (DEV_CONNECT_ERR)
12:39:35 : ST-LINK SN : 0015003A3156501620323443
12:39:35 : ST-LINK FW : V3J7M3
12:39:35 : Board : STLINK-V3MINI
12:39:35 : Voltage : 3.47V
12:39:35 : SWD freq : 8000 KHz
12:39:35 : Connect mode: Normal
12:39:35 : Reset mode : Software reset
12:39:35 : Device ID : 0x417
12:39:35 : Revision ID : Rev X
12:39:35 : UPLOADING OPTION BYTES DATA ...
12:39:35 : Bank : 0x00
12:39:35 : Address : 0x4002201c
12:39:35 : Size : 104 Bytes
12:39:35 : Bank : 0x01
12:39:35 : Address : 0x1ff80000
12:39:35 : Size : 20 Bytes
12:39:35 : UPLOADING ...
12:39:35 : Size : 1024 Bytes
12:39:35 : Address : 0x8000000
12:39:35 : Read progress:
12:39:35 : Data read successfully
12:39:35 : Time elapsed during the read operation is: 00:00:00.004
12:40:06 : Error: Unable to get core ID
12:40:06 : Error: Unable to get core ID
12:40:06 : Warning: Connection to device 0x417 is lost
12:40:08 : Disconnected from device.UPDATE 1: After the third time it does not disconnect anymore.. strange..
UPDATE 2:
Okay so upon comparing the two logs, I saw that CubeProgrammer is running at 8kHz while CubeIDE (set to auto) was trying 24kHz, I set it to 8 kHz and now it seems to work!
2021-07-17 3:45 AM
Sadly, I don't have another board. The necessary pins are connect (STM32CubeProgrammer works, see answer above)
2021-07-17 3:52 AM
No, it does not work on the next launches either..
I am using macOS Mojave 10.14.6 with STM32CubeIDE Version: 1.6.1 Build: 9958_20210326_1446 (UTC).
STM32CubeProgrammer is version 2.6.0 (Which seems to work, see my reply in answer below)
This is the gdb server log:
[0.000] initConfigParams(): Configuration flags start
[0.000] initConfigParams(): external-init false
[0.000] initConfigParams(): pend-halt-timeout (null)
[0.000] initConfigParams(): halt false
[0.000] initConfigParams(): config-file ""
[0.000] initConfigParams(): persistent false
[0.000] initConfigParams(): +log-file "/Users/linus/STM32IDE/bikelights2/Debug/st-link_gdbserver_log.txt"
[0.000] initConfigParams(): +log-level 31
[0.000] initConfigParams(): +port-number 61234
[0.000] initConfigParams(): +verbose true
[0.000] initConfigParams(): refresh-delay 15
[0.000] initConfigParams(): +verify true
[0.000] initConfigParams(): +swd true
[0.000] initConfigParams(): swo-port 61234
[0.000] initConfigParams(): cpu-clock 8000000
[0.000] initConfigParams(): swo-clock-div 128
[0.000] initConfigParams(): +initialize-reset true
[0.001] initConfigParams(): debuggers false
[0.001] initConfigParams(): +serial-number "0015003A3156501620323443"
[0.001] initConfigParams(): +apid 0
[0.001] initConfigParams(): attach false
[0.001] initConfigParams(): shared false
[0.001] initConfigParams(): erase-all false
[0.001] initConfigParams(): memory-map ""
[0.001] initConfigParams(): ext-memory-loaders false
[0.001] initConfigParams(): extload ""
[0.001] initConfigParams(): +stm32cubeprogrammer-path "/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.6.0.202101291314/tools/bin"
[0.001] initConfigParams(): temp-path ""
[0.001] initConfigParams(): preserve-temps false
[0.001] initConfigParams(): frequency -1
[0.001] initConfigParams(): licenses false
[0.001] initConfigParams(): ignore-rest false
[0.001] initConfigParams(): version false
[0.001] initConfigParams(): help false
[0.001] initConfigParams(): Configuration flags end
[0.001] init(): STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
[0.007] Device_Initialise(): Target connection mode: Under reset
[0.018] readFromTarget(): Reading ROM table for AP 0 @0xf0000fd0
[0.022] reset_hw_wtchpt_module(): Hardware watchpoint supported by the target
[0.025] Device_Initialise(): COM frequency = 24000 kHz
[0.025] Device_Initialise(): ST-LINK Firmware version : V3J7M3
[0.025] Device_Initialise(): Device ID: 0x417
[0.025] Device_Initialise(): PC: 0x0
[0.025] Device_Initialise(): ST-LINK Failed to get target status
[0.026] initServerContext():
Error in initializing ST-LINK device.
Reason: [0.026] initServerContext(): Unknown. Please check power and cabling to target.UPDATE:
Okay so upon comparing the two logs, I saw that CubeProgrammer is running at 8kHz while CubeIDE (set to auto) was trying 24kHz, I set it to 8 kHz and now it seems to work!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.