2021-07-20 10:47 AM
I wondering on which hardware configuration, I have to implement for this purpose.
Could I just use the differential pair as in joined picture without VBUS (as the µC is supplier on Board)?
I would like to get more details on how to design this interface and why shall I design it that way.
2021-07-20 11:23 AM
You can use the built-in bootloader like this, yes, but it doesn't have debugging capabilities. You'll also need to power it and a way of putting it into bootloader mode. Your signals are mislabeled, but the hardware connections are correct.
If you are developing a new board, you should include a SWD debug port to facilitate development.
2021-07-20 11:41 AM
Thanks for the prompt answer, mislabelling is ok as I wanted to know if it can work in that way.
For bootlaoder config, I use resistpor with assembly option for bootloader.
Programming over serial is also considered in the design.
What do you means by powering it? My µC is working with 3V3 and I do not want to include 5V on board, I thought using the differential pair like on firts picture can handle the problem.
Which of the option on tje joined could fit the case mention?
thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.