STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to program STM32G474RCT3 via JTAG

Hello,I'm working on a new project in which I'm using the new STMG series for development. At present, I'm trying to program the controller via JTAG. Unfortunately, the ST-Link is not able to connect to the controller. I'm attaching the screenshot of...

Resolved! Does StLink-v2 work on STM32L07?

I am currently working on STM32L07/STM32L08. And thinknig of debugging and making sure memory I would like to use st-link v2. I have looked up a lot about st-link but mostly it's about STM32F. Please teach me if the st-link v2 works on STM32L07/STM3...

SShir.2 by Associate II
  • 1428 Views
  • 2 replies
  • 0 kudos

Resolved! I am developing a product with a circuit using STM32L073RZT6. It is planned to be 3μA in the circuit design in STOP mode, but it can only drop to 40μA.

"When STOP mode is executed using the sample code of STM32CubeL0, the power consumption can be suppressed to 1 ~ 2uA, but it is the most consumed when the alarm and GPIO are enabled and the recovery from STOP mode is enabled. How can I reduce power c...

YHara.1 by Associate II
  • 1500 Views
  • 2 replies
  • 0 kudos

uC blocked in reset state

Hello,I am working on a custom board using a STM32F030K6T6. We are already in production and on like 15 parts over 4000, after that the product passed the electrical tests in production, and most of the time, after then, we tested it manually using ...

0693W00000D0mswQAB.png 0693W00000D0mtpQAB.png
JGreg.2 by Associate III
  • 1197 Views
  • 0 replies
  • 0 kudos

STM32H725 SMPS Issue

Hello,I designed a motor controller with an STM32H725ZG, and I am having problems withthe SMPS. First, with the board just assembled, the stm32CubeIDE let me uploada simple code (activating 25MHz crystal, debug, and blinking a led) one time.After upl...

0693W000008x1XGQAY.png
Adriialv by Associate
  • 2602 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.