STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f7508-dk HW upgrade issue

How can I port my stm32f7508-dk project from hardware C-02 to C-03when install the same binary file the screen will hang , that’s due to change in the flash memory ,now how to update the driver for flash memory g??thanks and regards

Makprog by Associate
  • 1457 Views
  • 2 replies
  • 0 kudos

LWIP working example for STM32F7508-DK

I have an STM32F7508-DK evaluation board. I would like to implement a simple web-server (http) on itbut none of the examples that I compiled seems to run on it.Do any of you have a simple LWIP+FreeRTOS working example for such a simple eval board? I ...

depSN by Associate
  • 1285 Views
  • 1 replies
  • 0 kudos

STM32 F030C8 interface LCD 16x2

Hi Everyone, I am trying to interface with LCD16x2 on STM32F030C8 custom board but I have some issues. I have LSE crystal on my custom board but HSE is not. When I debug my code, I have this problem: And when I run it, program does not work well and ...

volkan__0-1705996465702.png
volkan_ by Associate II
  • 2265 Views
  • 4 replies
  • 5 kudos

Resolved! QSPI in stm32h747 cm4

Hi community ,I'm currently working on STM32H747I DISCO0 Board .The peripheral I'm using is QSPI, I'm able to read/write and also enter Xip mode in CM7 .Problem:1)QSPI does not work in CM4 .Need to access QSPI in CM4 and perform same operations as re...

Resolved! STM32F103 UART interrupt not working

Hello, I'm building a project where I will use CAN, UART and a TIMER. All of these work with an interrupt. How it works: I get data via CAN and use a TIMER to send a Request on the CANbus. With the UART I need to receive some commands that will trigg...

Smdeint by Associate III
  • 6636 Views
  • 6 replies
  • 2 kudos

Hardware and software reference

Hi, STM32H743 development kit to develop my board.I want to develop my board in a way that each hardware interface can be selected between AI, AO, DI, DO by software. Is there any reference boards or reference documentations to implement such applica...

STM32F407 USB to UART

hello,Im trying to send the data I received on USB port (succesfully) to the UART port i tried sending data between 2 windows in Hercule, one is connected to the USB port, the other is connected to the UART port with the right configurations. I provi...

Lola_ by Associate II
  • 3276 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.