2024-01-24 1:27 PM
How can I port my stm32f7508-dk project from hardware C-02 to C-03
when install the same binary file the screen will hang , that’s due to change in the flash memory ,
now how to update the driver for flash memory g??
thanks and regards
2024-01-24 1:41 PM
Should be some metadata in the configuration for STM32 Cube Programmer command line to select
W25Q128JVEIQ_STM32F7508-DK.stldr
instead of
N25Q128A_STM32F7508-DISCO.stldr
2024-01-24 6:41 PM
Thanks for reply.
is it the same for the cubeIDE ?
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.