STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STWLC38 I2C Module

Hi there, should anyone recommend an I2C module for communicating with STWLC-GUI ??I have one already, but I need one more.Thanks.

JAKE2 by Associate III
  • 2279 Views
  • 2 replies
  • 1 kudos

Resolved! stm32 ADC scann mdoe

In the ADC scan mode in STM32 microcontrollers, the digitized value of all input channels is dumped into ADCx->DR. Is there a register or flags to find out which ADC channel the data currently in the ADCx->DR register```void HAL_ADC_ConvCpltCallback(...

Resolved! ST/LINK-V/2 STM32H723ZGT6 program 1st time

Trying to connect to a STM32H723ZGT6 for the first time. Does the ST/LINK-V/2 have to use the JTAG connection on this device as I feel it probably does? The 4 pin connection being for the STM8 only? I jave connected as a JTAG connection using jumper ...

MDeac.1 by Associate III
  • 4223 Views
  • 4 replies
  • 1 kudos

Resolved! Nucleo-F303RE want to set timer source muxes to use PLLCLK*2, to yield 2 * 72 MHz=144 MHz resolution

I'm on Nucleo-F303RE board, which according to the page 129-130 of the reference manual (RM0316 Rev 10) I should be able to set "TIMx (x = 1/2/3/4/8/15/16/17/20) can be clocked from the PLL running at 144 MHz when the system clock source is the PLL a...

ericfont_2-1705608111890.png ericfont_0-1705607810460.png
ericfont by Associate II
  • 2577 Views
  • 3 replies
  • 2 kudos

Hall sensor/ encoder

Hi Team,Could anyone please suggest which hall sensor or encoder is supported for the P-Nucleo-IHM03 board. I have generated the code for the hall sensor feedback but not able to find the suitable sensor.Anyone who have used the board please suggest....

STM32F407VET6 and a 7" display

I am trying to design a system that use the STM32F407VET6 and a 7 inch LCD display that use LVDS. The screen is 1024x600 pixel resolution and can use 6-bit or 8-bit LVDS interface. The screen also uses a HX8282 LCD controller. I was wondering if I ne...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.