STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to program clone ST-Link V2.1

Hi, I am making my clone ST-Link v2.1 device using 128 KB STM32F103CBT6 mcu. Please help clarify as follows: 1) Do I need to set Boot 0 pin = 1 and Boot 1 pin = 0 in order to program the bootloader into the device?2) Do I need to set Boot 0 pin = 0 a...

STehA.1 by Associate II
  • 5651 Views
  • 2 replies
  • 1 kudos

STM32G474 discovery kit no voltage at Vin

Hi all, I am trying the voltage mode buck converter provided by ST with my STM32 discovery kit. I followed the instructions from an5497-buck-current-mode-with-the-bg474edpow1-discovery-kit-stmicroelectronics.pdf and the program files are directly dow...

OFN by Associate II
  • 1915 Views
  • 2 replies
  • 0 kudos

The stm32 is not supplied with current.

Hi, I designed stm32f413RGT6. But when I supplied 5V as a power supply, I only get 0.00~0.01A.When I measure with a multimeter, the chip has a voltage of 3.3V.I think it's a problem caused by not connecting VCAP1, so I connected 4.7uF to VCAP1 with G...

B-G474E-DPOW1 does not connect to PC

I am trying to connect to the B-G474E-DPOW1 developement kit with my PC, i followed the steps reported in the um2577 LD6 and LD7 light up but the led LD9 remains off, what could be the issue?I correctly installed the ST-LINK drivers, i tried to updat...

0693W00000HptLnQAJ.png 0693W00000HptLyQAJ.png
MColu.1 by Associate II
  • 3275 Views
  • 4 replies
  • 1 kudos

Resolved! STM32F407 Discovery 1 board - CAN support

Hello,I am new to STM parts. We are using STM32F407 Discovery 1 evaluation boards. I was wanting to configure the two boards to communicate over CAN with one another.In STMCubeMx, I select the STM32F407 Discovery 1 board and see the following that CA...

Untitled.png
BAW by Associate III
  • 2563 Views
  • 2 replies
  • 2 kudos

STM32 LD1 Blinks and LD3 remains red

Hello guys, I have Nucleo F072RB, when I first bought it, it works fine when I plug it to PC. But today, When I plugged USB cable, LD1 blinks in approximately 1 HZ and LD3 remains red. I have searched it on the internet but I couldn't find a solution...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.