STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No STM32 Found on ST Link V2 JTAG Port

Before ST started bricking counterfeit st link V2 units, I was able to program my board without issue. I bought a confirmed genuine ST Link V2 from RS components and connected it exactly as shown, but it never connects to the target and all I can get...

st.png
sdobbie by Associate II
  • 3846 Views
  • 4 replies
  • 1 kudos

Nucleo-L152RE cellular shield

Hello !I looking for a cellular shield for my project that would fit on my Nucleo-L152RE board. Does the ST company produce something similar and is it possible to buy it ?   Sincerely,Maxim 

Max75 by Associate II
  • 1124 Views
  • 1 replies
  • 0 kudos

STEVAL-CTM011V1 & X-CUBE-MCSDK

HiI'm following the UM2692 to start a develop with the STSPIN32F060x.I just have the STEVAL-CTM011V1A board and the STLINKV3 with the isolator adapter and a 1/6HP three phase motor.I started the "Fimware Debug" part on the UM2692, page 7.Perform the ...

PGinhson by Associate III
  • 2626 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H573 & RS232

Hello Everyone, I am using STM32H573. Do we need to connect RS232 to UART transceiver or can we directly interface Rs232 signals with UART?

madhu1 by Associate II
  • 2951 Views
  • 4 replies
  • 3 kudos

Resolved! XIP mode in CM4

HI, community I'm working on QSPI FLASH in STM32H747I DISCO ,i was able to access XIP mode in M7 .Currently I'm trying to work on M4 tried XIP mode in CM4 but there isn't cache in M4 ,and i was not able to access XIP mode .Is the cache the issue or s...

Resolved! Problem with loops on STM32F103C8T6

Hello! I’m using Keil uVision to program the stm32f103c8t6 (blue pill). I’m having problems with the loops when trying to turn on and off the LED on pin 13 port C. I just wanted to use a loop to generate a delay without needing to use timers, since I...

Resolved! How to find GPIO pin for Adc module

Hello everyone,i want to config gpio pin as adc chanels on stm32f103c8t6, i have read the GPIO chapter and ADC chapter,but i can not find out what is GPIO pin for each ADC chanel,example GPIOA_pin0 for ADC1_chanel0...,what is the chapter describe abo...

BinhTsks by Associate II
  • 2886 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.