Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi ST TeamI have added a sensor implementation to the FP-SNS-DATALOG2 (2 D movement tracking sensor PAT9136) in order to be able to record position data together with MEMS sensor data. This works well for data recording/retriving to/from the SD card....
I want to connect B-CAMS-OMV (cam module ) to B-U585-IOT02A ( discovery kit). But there is no info bout that connection. I already read the user guide bout both. Can you give me some information or solution bout Connection with B-CAMS-OMV and B-U585-...
Can I get a site or link about buying CN7 connector for B-CAMS-OMV & B-U585-IOT02A ?
Dear Billy I have a similar problem. I can't order the board NUCLEO-H563ZI. The error is: "Your cart is not eligible for this promotion. Ensure that you are logged in and items match promotion terms. For help, contact ST Support." Please help me solv...
HiI have a problem with my board with STM32L496ZGT6.Some boards works fine (so.. i think there isn't a project problem) some boards are in loop during the power on.I exaplin better:Here a function in main.cpp: /*Configure the main internal regulator...
Hallo,until now we have used STLINK-V3SET connected with MIPI10 to custom evaluation board based on STM32H743.For next custom board we need cost efficient debugger solution, just like STLINK-V3MODSBut it seems not to work together.MIPI10 connector us...
Hello,I have finally received a voucher to get a free NUCLEO-H563ZI board when attended workshop "STM32H5: Ultimate combination of performance, integration and affordability".Despite following the procedure provided in mail I'm unable to get past Pla...
Hi,We are now using NXP mcus for our smart lighting products, and decide to use STM32 mcus for instead from now, I bought one Nucleo-STM32G070, one Nucleo-STM32F103, and one Nucleo-STM32F767. The most challenging work for us is to build a TCP/IP appl...
Hello everyone, I hope you're all doing well. Recently I have tried to measure temperature using a K-type thermocouple with a breakout board that uses a MAX31855 IC Its sends out 32 bits and my board can read 32 bits SPI. I have wired everything corr...
Hello FreeRTOS friends,I'm back seeking guidance. I want to mention that I've configured this project without using the IDE, by manually setting up the necessary ETH pins for its operation.I've followed the documentation on the page, but I'm unable...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.