2024-02-02 10:29 AM
Hi
I'm following the UM2692 to start a develop with the STSPIN32F060x.
I just have the STEVAL-CTM011V1A board and the STLINKV3 with the isolator adapter and a 1/6HP three phase motor.
I started the "Fimware Debug" part on the UM2692, page 7.
Perform the code generation step by step with the Workbench, then the MX and then download the firmware with the X-Cube IDE following the steps one by one. Once the program is loaded in STEVAL, I return to the workbench and try to run it with the workbench start button as already explained to me, but I get no results. Looking, I see that the workbench does not connect to the STEVAL board; I left it connected to the STLINK through the SWD where I programmed it. What am I doing wrong? I don't know if I should establish communication through a different port, I can't find that clarification anywhere.
Thank you for your patience, I am new to ST, I have been using other brands for many years and I am not yet 100% familiar with these tools.
2024-02-02 11:47 AM
2024-02-02 11:59 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.