Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I have the x-nucleo-GFX01M2 LCD which is compatible with my nucleo 64 board (F103RB). I am wondering how best to get started with graphics on this LCD, as there are no examples in the X Cube Display 3.0.0. for this board. The examples are for some G,...
Hello I have been using an STLink v3 pod successfully for several months but suddenly it stopped working. The green light is lit and the red one flashes slowly. I cannot see it in Device Manager and there are no Unknown Devices. There is no chime...
Hello, I would like to interface STM32U5G9 with SD Card. Looking at SensorTileBox.Pro schematic, I see that an SD Card Driver (st6g3244mebjr) is placed in the middle. What is the added value in using it? Thank you
Hello,I am having trouble getting the USB peripheral recognized by the PC device manager. In Cube I have the USB FS device checked, and the USB_DEVICE middleware set to virtual COM port. Everything else is set to default.The USB clock is set to 48M...
HiI use STM32 NUCLEO-H743ZI2 development board for my project. I'm considering purchasing electronic components for the first time, and I would appreciate a recommendation for an X3 crystal that could be used in this situation.Additionally,I understa...
I have a couple of questions regarding the ADC clock on the board in the subject.What is the default clock speed and where is the clock configured?All I see in the documentation is that the clock is independent from the AHB clock, but I don't see whe...
I'm pretty new to using USB in Stm32, and I wanted to read the variables through a USB-C connected to the controller. StmcubeMX provided me with an initialization code. After flashing this code, the comp port is not showing on the system. I have atta...
Hi guys, I was trying to implement CAN in STM32F429I-DISC1. In that board when using PB5 and PB6 for CAN2 it is working but when using CAN2 with PB12 and PB13 it is not working and it shows bit dominant error. if any of you faced this er...
Hello, I ty to configure the clock setup of stm32f407 board using registers .But I am not getting the values of Registers in the SFR while debugging.Since I am enabling the GPIOD in the AHB1ENR registers but still I am not getting the value during th...
Hello, looking to see if it is possible to connect a IR transmitter and receiver to a stm32f429zi nucleo board. Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.