Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Dear STM support team.My name is Dai. I am working at G-innovation Corporation.Now I have a project using the STM Chip(STM32F0xx).I use the STM32CubeMX (version 6.11.0) to create a project using the STM32F091VBT6 with CMIS_RTOS.this project aims to s...
I am trying to communicate(Tx and Rx) with the arduino serial monitor using USART2 using ppins PA2 and PA3 respectively. This si done with the assumption that these are the pins which are connected to the USB serial wires. Mt USART Tx fucntion is wor...
Hello All,I bought the NUCLEO-F446ZE board and would like to use Ethernet port but it is not soldered onto the board.Which RJ45 jack do I need to buy? Could someone provide reference to Mouser or Digikey?
Hello All,I would like some clarification as to how I can verify if the internal clock HSI will run based on what external power input is given.I had originally found that running the board on external 3.3 v will not allow the HSI clock to be used, a...
Hello everyone!I am working with STM32H7B3I-DK and I have enabled USART1 based on the available example, but I need to enable USART2 to connect to the WiFi. If I use the same code but with RX and TX pins from USART2, I can see nothing on console. Do ...
Hi Guys I'm Trying to find stm32l073rz Nucleo board datasheet that contains the boards pin description, but I can't find it anywhereI have found those but when I compare the pin description in the first pic from: NUCLEO-L073RZ | Mbedwith the one prov...
Greetings,I have recently purchased an STEVAL-IDB012V1A evaluation board. I can display the Pressure and Temperature but no data for the accelerometer and gyroscope. Does anyone experienced the same problem or may I have a faulty board ?Thanks.
I recently designed an stm32 board based on the stm32f4 I used a multimeter to test all the vdds and nrst everything is normal 3.3V but the vcaps only show 0.3V instead of 1.2V, what could be the problem? Can anyone help?
Hello,I purchased a soldering crystal for X3 according to the BOM list,but it seems that the X4 on the board is the same product.Where is the X4 used?I checked UM2407 User Manual and STM32H742xI/G, STM32H743xI/G datasheets,but couldn't find it. Plus,...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.