2024-04-18 5:00 AM
Hello,
I would like to interface STM32U5G9 with SD Card. Looking at SensorTileBox.Pro schematic, I see that an SD Card Driver (st6g3244mebjr) is placed in the middle. What is the added value in using it?
Thank you
Solved! Go to Solution.
2024-04-18 6:43 AM
The ST6G3244MEBJR (U16) is used as a level translator from 1.8V to 3.0V.
Does it answer your question?
Regards
/Peter
2024-04-18 6:43 AM
The ST6G3244MEBJR (U16) is used as a level translator from 1.8V to 3.0V.
Does it answer your question?
Regards
/Peter
2024-04-18 6:50 AM - edited 2024-04-18 7:17 AM
That's ok.
I double checked the topic and, as the SD Card initial communication voltage level is at 3.3 V (only when switching to UHS-I changes to 1.8 V), we need for a certain initial time to shift communication to 3.3V. In SensorTileBox.Pro the STM32U5 is powered at 1.8 V. I hoped that the voltage level change could be managed directly by STM32U5, but it is stated the an external voltage level translator is needed.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.